Setting the Scene
Best known for manufacturing manhole covers, a well known foundry has
been supplying quality castings for the last 135 years. A typical foundry
deals in harsh environments, and this one was no exception. Metal
particulates and other contaminants make smooth linear motion difficult
throughout the production process.
PBC Linear came into contact with the customer after they were
experiencing problems with their production lines. The casting tipper is
used to divert a number of foundry castings after they have been molded;
however the machine was experiencing massive downtime on account of
failing cam followers. This caused the production line to fail and production
costs to increase. Due to the harsh nature of the environment, and the
massive load and force required to move the castings, PBC Linear
recommended their Hevi-Rail system.
The Challenge
The production lines at the foundry are long and carry dozens of castings
at a time. This load weighs tons and requires incredible force in order to be
moved. The foundry attempted to use other heavy duty linear guide
systems to restore the casting tipper; however they were not durable
enough and failed within two weeks. PBC Linear was faced with the task of
producing a solution that allowed the casting tipper to function properly
with immense force and load without repeated failure.
The Solution
With its strong load capacity and ability to last in harsh environments,
Hevi-Rail was the perfect solution. Hevi-Rail’s design disperses the weight
and allows for the system to carry a massive amount of load without
failure.
The Hevi-Rail system has kept the production lines running for 1-1/2 years
and continues to function efficiently. As a result, the customer has
experienced huge cost savings due to the lack of downtime and
catastrophic failure.
Products Used
HVB056, HBP-2 and HVR-2 rail were all implemented into the foundry’s
casting tipper and continue to function properly.
For more information on the Hevi-Rail and all its features, please call 1.800.729.9085, or send an email to marketing@pacific-bearing.com. |